AOUT#.VALUEU
Description
Gets or sets the user command value of the specified analog output when AOUT#.SOURCE = 0 (user).
Examples
Usage
When AOUT#.SOURCE = 0 (user) then the corresponding AOUT#.VALUEU is used to drive the AOUT#.VALUE .
Code
Changing output value with VALUEU and then changing SOURCE to be action table with no action configured:
--> AOUT1.SOURCE 0 //user --> AOUT1.VALUEU 0.000 V --> AOUT1.VALUE 0.000 V --> AOUT1.VALUEU 1 --> AOUT1.VALUE 1.000 V
Context
For more information see Analog Output.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | V |
| Range | 0 to 10 |
| Default Value | 5 |
| Data Type | Float |
| See Also | |
| Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
| FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AOUT1.VALUEU | 0x3800 | 0x2 | INT | 1000:1 | - | RW | True |
| AOUT2.VALUEU | 0x3801 | 0x2 | INT | 1000:1 | - | RW | True |
|
Copyright © 2018 Kollmorgen |
|